/*
uf_clsf.h
File Description:
Contains Open C API for the NX Oper module.
******************************************************************************/
#ifndef UF_CLSF_H
#define UF_CLSF_H
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_cam.h>
#include <libufun_cam_exports.h>
/********************************** Defines ***********************************/
/******************************* Prototypes **********************************/
/*****************************************************************************
* Function Name: UF_CLSF_import
*
* Function Description:
* This function imports the CLS tool paths into the part specified
*
******************************************************************************/
extern UFUN_CAMEXPORT int UF_CLSF_import
(
tag_t part_tag, /* <I>
the NX part tag
*/
char *clsf_name /* <I>
the name of the cls file from which the tool paths are imported
*/
);
#undef EXPORTLIBRARY
#endif