/*
uf_cam_spec.h
File description:
This file contains the documentation for the pre-v16 UF_CAM module.
UF_CAM_exit_id_t is the identifier type that is passed between NX CAM and a
User Exit. This identifier is only used upon the original call to the User
Exit. After receiving this identifier the User Exit must call
UF_<module>_ask_<module> to retrieve the identifier which will be used in
further transactions with NX CAM via the User Function layer for a
particular module.
******************************************************************************/
#ifndef UF_CAM_OLD_H
#define UF_CAM_OLD_H
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
/********************************** Defines ***********************************/
/********************************** TypeDefs **********************************/
/****************************************************************************
This is the identifier type that is passed between NX CAM and a User
Exit. This identifier is only used upon the original call to the User
Exit. After receiving this identifier the User Exit must call
UF_<module>_ask_<module> to retrieve the identifier which will be used in
further transactions with NX CAM via the User Function layer for a
particular module.
*****************************************************************************/
typedef void *UF_CAM_exit_id_t;
/******************************* Prototypes **********************************/
#endif