UF_CUT_LEVEL_single_s (view source)
 
Defined in: uf_cut_levels.h
 
Also known as:
 
Overview
Data structure for a single cut level.


Data Members

entity_tag
tag_t
Tag id of the face or point entity
used to define the current cut level.
This can be NULL if the level was
defined by an explicit z level.

z_level
double
The z distance of the cut level from the
origin along the normal of the cut levels.

local_cut_depth
double
The max depth per cut value to be
used for the range between this cut
level and the one above it.