UF_CAMBND_app_data_s (view source)
Defined in: uf_cambnd.h
Also known as:
- UF_CAMBND_app_data_t
- UF_CAMBND_app_data_p_t
Overview
The application data for a boundary and the members:
The following information shows the types of application data
allowed by the objects and the boundary types.
An error code is returned by the functions if a wrong type
of application data is set.
Facing Operation Boundary:
Blank Boundary:
Boundary: Stock, Feedrate
Boundary members: Stock, Feedrate, Tool Position
Check Boundary:
Boundary: Stock, Feedrate
Boundary members: Stock, Feedrate, Tool Position
Planar Mill Operation Boundary: (also Cavity Mill)
Part Boundary:
Boundary: Stock, Tolerances, Blank Distance, Feedrate
Boundary members: Stock, Tolerances, Feedrate, Tool Position
Blank Boundary:
Boundary: Stock, Tolerances, Feedrate
Boundary members: Stock, Tolerances, Feedrate, Tool Position
Check Boundary:
Boundary: Stock, Tolerances
Trim Boundary:
Boundary: Stock, Tolerances
Data Members
has_stock
int
stock
double
has_tolerances
int
tolerances [ 2 ]
double
has_feedrate
int
feedrate_unit
feedrate_value
double
has_blank_distance
int
blank_distance
double
has_tool_position
int
tool_position
Set to 1 if used, or else set to 0.