/*
uf_attr.h
File description:
This is the Open API interface to part and object attributes.
Using the UF_ATTR subroutines, you can:
. Assign an attribute title and value to an object.
. Count the attributes with a specific type for an object.
. Cycle through all attributes of a specific type from an object.
. Delete an attribute of a specific type from an object.
. Delete all attributes of a specific type from an object.
. Search an object for a specified attribute title.
. Read the value of an attribute with a specified type and title.
The API consists of two subsets, a post-NX8 set and a pre-NX8 set.
The pre-NX8 set.
The pre-NX8 set (legacy) set supports applications written against pre-NX8 versions of NX.
We have tried to make sure that such applications can continue to function without changes.
The functions in this set do not have string 'user_attribute' as part of the name.
It does not support some of the new enhancements that were introduced in NX8
during a major restructuring of the user attribute functionality. This set also
treats PDM-based attributes (attributes that are mapped to and from the
Teamcenter PDM system) differently from other attributes, as follows:
a. Reading a set PDM-based attribute will return it as being of string type
independent of its actual type. The actual value will be converted to a
string using conversions similar to those converting PDM-based attributes
to string type prior to NX8.
b. An attempt to read an unset PDM-based attribute will return it a set
attribute of string type with an empty string as its value.
c. Setting a PDM-based attribute requires that the input be of string type.
The actual value will be converted to a value of the actual type prior
to creating an attribute of that (the actual) type.
d. Setting a PDM-based attribute with an empty string as input will remove
the attribute from NX.
The post-NX8 set.
The expanded set supports a number of enhancements that were introduced in NX8
during a major restructuring of the user attribute functionality. This set
is labelled 'recommended' below. All the functions in this set have the string
'user_attribute' as part of the name.
This set can be used to by legacy applications to take advantage of the
NX8 attribute enhancements or it can be used to build new applications.
**********************************************************************************
Unset Attributes
Some functions in this API will return values for 'unset' attributes. While an
object has a virtual infinity of unset attributes, the ones returned by this API
are restricted to titles for which the object has an associated attribute template.
If there is no attribute, but there is a template, then the attribute is said to be
'unset'.
As noted above, the pre-NX8 API does not support this concept. Instead it will
treat all 'unset' PDM-based attributes as 'set', but empty, string attributes.
The post-NX8 API fully supports the notion of 'unset' attributes.
**********************************************************************************
Object Tags
The functions in this file will accept the tag of any object that supports attributes.
The tags for a part object or for a part attribute object (UF_ATTR_ask_part_attribute) can be
used interchangeably.
**********************************************************************************
Units
When setting attributes with units, the functions here require the tag of a unit type.
These tags can be obtained via the UNIT API (see uf_unit.h).
The UNIT API also allows for the conversion of values between compatible units.
When reading an attribute with units, the functions here will return the value in
the display units of the attribute and those units are returned, with one
exception, as a tag. When reading part attributes from a file, the unit tag becomes
invalid during the call, so a NULL tag is returned.
In addition to a unit tag, a string with the unit name is returned.
The name returned is the untranslated name of the units.
**********************************************************************************
NX Date & Time Formats
NX computational date and time is stored in an integer array consisting of two
elements. The first array element contains the NX Computational Date, while
the second contains the NX Computational Time.
NX Computational Time stores the number of six second intervals since midnight,
that is it is incremented every six seconds. The computation is:
NX_computations_time = 10* (60*Hour+Minute) + Second/6
where Hour = Hour of day on 24 hour clock and Minute = Minute of hour, and
Second is the Seconds of the minute.
NX also allows for time attribute values to be entered and read via a formatted string.
In order to understand such formatted strings, NX needs to know the format used to create them.
The time to string conversion format is set via the following environment variable:
'UGII_DEFAULT_DATE_ATTRIBUTE_DISPLAY_FORMAT'
It can also be set via this API (UF_ATTR_set_time_string_format).
Further, when NX is run in managed mode, then Teamcenter may also provide a format via the preferences 'NXDefaultDateFormat' (preferred) or 'DefaultDateFormat'.
The following describes the syntax of the format string. Constant strings may be interspersed between tokens.
%b abbreviated month name
%B full month name
%d day of the month(0-31)
%H hour(24-hour clock)(00-23)
%I hour(12-hour clock)(01-12)
%m month(01-12)
%M minute(00-59)
%S second(00-59)
%y year without century(00-99)
%Y year with century(1970-2069)
Example:
%d-%b-%Y %H:%M:%S is the format that gives 01-Mar-2011 22:16:32
If no format is set, then the example format is used by default.
**********************************************************************************
Locks
To enable an NXOpen program to modify the locks of an attribute, the user name under which the
program is run must have privilege to do so. This privilege is set via the
Customer Default option
'UG_AllowAttributeLockingInNXOpen'
**********************************************************************************
Reference Strings
In NX8, reference type attributes (UF_ATTR_reference) are no longer supported as a different type.
These attributes are converted to string type with references to a string expression that
implements the formula describe the reference string.
When these attributes are read, the string expression formula is converted back
to a reference string.
When a reference string has a token that picks up a value from a number expression that
has units, then the resulting expression formula is created to format the expression's value
using the display units at the time of the creation of the referenced expression. This
formula does not change if the original expression's display units change. However, the
formula can be manually edited in the expression dialog as needed. Alternatively, the
attribute can be reset, at which time it will gain the new units.
**********************************************************************************
Templates
There are currently no plans to support the creation of templates in this API.
**********************************************************************************
Material and Mass Property Related System-Owned Attributes
Prior to NX10, certain system attributes had their titles defined
via Customer Defaults. In NX10, they were given hard-coded titles and aliases defined
via Customer Defaults.
Given that external applications may be looking for these attributes via
their old titles, the functions in this API that specifically looks for attributes
via a title will work when given an alias of one of these attributes.
We list here the new hard-coded titles together with the old default titles and
new default aliases. If, prior to NX10 you used
titles other than the defaults, then for this to work you need to set the new
alias to the same as what the titles were set to before.
New Title Old Default Title and New Default Alias
---------------------------------------------------------------------
NX_Material Material
NX_ObjectMaterial ObjectMaterial
NX_MaterialMultipleAssigned MaterialMultipleAssigned
NX_MaterialMissingAssignments MaterialMissingAssignments
NX_MaterialPreferred MaterialPreferred
NX_MassPropDensity MassPropDensity
NX_MassPropMass MassPropMass
NX_MassPropWeight MassPropWeight
NX_MassPropVolume MassPropVolume
NX_MassPropArea MassPropArea
NOTE: No other attributes than those converted in this way by Siemens will
be able to be reached by this API via an alias. Using aliases in applications
is not recommended because aliases can change. In fact the above mentioned changes
were partly made to ensure that access to these attributes by applications be
independent of the Customer Default settings. Using aliases also has
performance impacts because of the need to search for matching titles. Lastly,
in some applications it is possible for attributes to share aliases, so
an attribute cannot in all cases be uniquely identified via an alias.
Refer to definition of constants
that should be used in your source code when appropriate.
*/
#ifndef UF_ATTR_INCLUDED
#define UF_ATTR_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_attr_types.h>
#include <libufun_exports.h>
/*****************************************************************************
* UF_ATTR_init_user_attribute_info
*
* Initializes a UF_ATTR_info_t struct as follows:
*
* All strings are set to NULL.
* All numerical values are set to 0 or 0.0.
* All logical values are set to false.
* All tags are set to 0
*
* NOTE: This function must be called before the struct can be used
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_init_user_attribute_info
(
UF_ATTR_info_p_t info /* <I/O> the attribute information to be initialized */
);
/*****************************************************************************
* UF_ATTR_free_user_attribute_info_strings
*
* Frees the strings held by a UF_ATTR_info_t struct.
*
* All strings held by the struct are freed.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_free_user_attribute_info_strings
(
UF_ATTR_info_p_t info /* <I/O> the attribute information containing strings to be freed */
);
/*****************************************************************************
* UF_ATTR_free_user_attribute_info_array
*
* Frees the strings held by an array of UF_ATTR_info_t structs as well as the array itself.
* (Use after call to UF_ATTR_get_user_attributes)
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_free_user_attribute_info_array
(
int count, /* <I> the count of attribute information structs in the array */
UF_ATTR_info_t info[] /* <I> the array of attribute information structs to be freed */
);
/*****************************************************************************
* UF_ATTR_init_user_attribute_iterator
*
* Initializes a UF_ATTR_iterator_t struct as follows:
*
* All strings are set to empty.
* All logical values are set to 'false'.
* The 'type' is set to 'UF_ATTR_any'.
* The 'array_element_index' is set to 'UF_ATTR_ANY_ATTRIBUTE'
*
* NOTE: If the info has pointers to strings that it does not own, such strings must be
* set to NULL before this function is called.
*
* Environment: Internal and External
* See Also: Refer to example
* History: NX8.5.3
******************************************************************************/
extern UFUNEXPORT int UF_ATTR_init_user_attribute_iterator
(
UF_ATTR_iterator_p_t iter /* <I/O> the attribute iterator to be initialized */
);
/*****************************************************************************
* UF_ATTR_release_user_attribute_iterator
*
* Resets and releases for re-use a UF_ATTR_iterator_t struct.
*
* This must be done in two situations:
*
* a. Before the iterator is to be reused for another iteration.
* b. When the iterator is no longer in use
*
* This function does not free the strings supplied with the iterator or the iterator itself,
* but it does free internal memory associated with the iterator.
*
* If a release is not done after the iteration is completed, the iterator may
* produce unpredictable results when reused.
* If a release is not done after the iterator is retired, the iterator will leak internal memory.
*
* NOTE: Releasing an iterator twice is OK.
* Iterations that are always completed (such when used in UFT_ATTR_has_user_attribute())
* will automatically release the iterator. Please see the individual functions for details.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
******************************************************************************/
extern UFUNEXPORT int UF_ATTR_release_user_attribute_iterator
(
UF_ATTR_iterator_p_t iter /* <I/O> the attribute iterator to be released */
);
/*****************************************************************************
* UF_ATTR_free_user_attribute_iterator_strings
*
* Frees the strings held by a UF_ATTR_iterator_t struct.
*
* All strings held by the struct are freed.
* Note: The UF_ATTR API does not supply the strings held by this struct, this
* function for convenience only.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_free_user_attribute_iterator_strings
(
UF_ATTR_iterator_p_t iterator /* <I/O> the attribute iterator containing strings to be freed */
);
/*****************************************************************************
* UF_ATTR_set_time_string_format
*
* Sets the format used to convert a time attribute value to a string (and vice versa)
* This function will override (replaces) any format set via the environment variable 'UGII_DEFAULT_DATE_ATTRIBUTE_DISPLAY_FORMAT'.
* To allow setting a format temporarily, this function returns the existing format.
* The given format is a string that has the following tokens. Interspersed text will be copied:
* %b abbreviated month name
* %B full month name
* %d day of the month(0-31)
* %H hour(24-hour clock)(00-23)
* %I hour(12-hour clock)(01-12)
* %m month(01-12)
* %M minute(00-59)
* %S second(00-59)
* %y year without century(00-99)
* %Y year with century(1970-2069)
*
* Example:
* %d-%b-%Y %H:%M:%S is the format that gives 01-Mar-2011 22:16:32
*
* If no format is set (via the environment variable or via this function), then the example format is used by default.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_time_string_format
(
const char *new_format, /* <I> The new format to be used */
char **old_format /* <OF> The format previously in used (optional - may be NULL.
If not NULL, the caller is responsible for freeing the returned old format string.
Free using UF_free() after use.*/
);
/*****************************************************************************
* UF_ATTR_set_user_attribute
*
* Creates or modifies an attribute with the option to update or not.
*
* NOTE: To set a date/time type attribute, either a formatted string or a computational value may be used.
* If both are set (the string is not empty ("") and the computational value is not (0,0)), then the computational value will take precedence.
* The time value in either case is in the current time zone of the machine running the program.
*
* NOTE: To set a real type attribute, there is the option to include a units specification.
* The supplied 'unit_type' must be consistent with the unit specification of an existing attribute or template with same title.
* In other words, the attribute's unit measure cannot change, but its display units can.
* If 'unit_type' is not supplied (the tag is NULL_TAG)
* If an existing attribute or template is found, then the units of that attribute or template are used.
* If no existing attribute or template is found, then the attribute is set to be unit-less.
* If 'unit_type' is supplied:
* If an existing attribute is found, then that attribute's display unit is modified to use the input 'unit_type'.
* If no existing attribute is found, then the attribute is created with the given 'unit_type' as its display units.
*
* Replaces: UF_ATTR_assign
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const UF_ATTR_info_t *info, /* <I> The attribute information for the attribute (make sure to initialize it first) */
logical update /* <I> Perform an update immediately */
);
/*****************************************************************************
* UF_ATTR_set_null_user_attribute
*
* Creates a null type attribute with the option to update or not.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_null_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
logical update /* <I> Perform an update immediately */
);
/*****************************************************************************
* UF_ATTR_set_boolean_user_attribute
*
* Creates a boolean type attribute with the option to update or not.
*
* Environment: Internal and External
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_bool_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
logical value, /* <I> The value */
logical update /* <I> Perform an update immediately */
);
/*****************************************************************************
* UF_ATTR_set_integer_user_attribute
*
* Creates a integer type attribute with the option to update or not.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_integer_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
int value, /* <I> The value */
logical update /* <I> Perform an update immediately */
);
/*****************************************************************************
* UF_ATTR_set_real_user_attribute
*
* Creates a real type attribute with the option to update or not.
*
* NOTE: The supplied 'unit_type' must be consistent with the unit specification of an existing attribute or template with same title.
* In other words, the attribute's unit measure cannot change, but its display units can.
* If 'unit_type' are not supplied (set to NULL_TAG), then:
* If an existing attribute or template is found, then the units of that attribute or template are used.
* If no existing attribute or template is found, then the attribute is set to be unit-less.
* If 'unit_type' are supplied, then:
* If an existing attribute is found, then that attribute's display unit is modified to use the input 'unit_type'.
* If no existing attribute is found, then the attribute is created with the given 'unit_type' as its display units.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_real_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
double value, /* <I> The value */
tag_t unit_type, /* <I> The unit type tag (may be NULL_TAG) */
logical update /* <I> Perform an update immediately */
);
/*****************************************************************************
* UF_ATTR_set_string_user_attribute
*
* Creates a string type attribute with the option to update or not.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_string_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
const char *value, /* <I> The value */
logical update /* <I> Perform an update immediately */
);
/*****************************************************************************
* UF_ATTR_set_reference_string_user_attribute
*
* Creates a string type attribute with the option to update or not.
* This string attribute will be created with the given reference string.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_reference_string_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
const char *reference_string, /* <I> The reference string */
logical update /* <I> Perform an update immediately */
);
/*****************************************************************************
* UF_ATTR_set_computational_time_user_attribute
*
* Creates a time type attribute with the option to update or not.
*
* The time value must be entered in the current time zone of the machine running the program.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_computational_time_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
int value[2], /* <I> The time value {day,min} */
logical update /* <I> Perform an update immediately */
);
/*****************************************************************************
* UF_ATTR_set_string_time_user_attribute
*
* Creates a time type attribute with the option to update or not.
*
* The time value in either case is in the current time zone of the machine running the program.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_string_time_user_attribute
(
tag_t object, /* <I> The object receiving the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
const char *value, /* <I> Time/Date value as a formatted string */
logical update /* <I> Perform an update immediately */
);
/****************************************************************************
* UF_ATTR_get_user_attribute_lock_with_title_and_type
*
* Gets the information from the attribute with the given title and type
*
* Replaces: UF_ATTR_ask_locked
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_user_attribute_lock_with_title_and_type
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int type, /* <I> The attribute type
Valid values:
UF_ATTR_integer
UF_ATTR_real
UF_ATTR_time
UF_ATTR_null
UF_ATTR_string
UF_ATTR_bool
UF_ATTR_any
NOTE: If UF_ATTR_any is used, the first attribute encountered that matches
the given title (and index), is returned
*/
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
logical *is_locked, /* <O> The lock status of the attribute. Valid only if the attribute is set. */
logical *has_attribute /* <O> A set attribute has been found*/
);
/****************************************************************************
* UF_ATTR_get_user_attribute_with_title_and_type
*
* Gets the information from the set attribute with the given title and type
*
* Replaces: UF_ATTR_read_value, UF_ATTR_read_reference_string, UF_ATTR_find_attribute
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_user_attribute_with_title_and_type
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int type, /* <I> The attribute type
Valid values:
UF_ATTR_integer
UF_ATTR_real
UF_ATTR_time
UF_ATTR_null
UF_ATTR_string
UF_ATTR_bool
UF_ATTR_any
NOTE: If UF_ATTR_any is used, the first attribute encountered that matches
the given title (and index), is returned
*/
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
UF_ATTR_info_t *info, /* <OF> The attribute information for the first set attribute found, if any.
This struct must be freed using UF_ATTR_free_user_attribute_info_strings() after use. */
logical *has_attribute /* <O> A set attribute has been found*/
);
/****************************************************************************
* UF_ATTR_get_user_attribute_lock
*
* Gets the lock information from the first attribute, that satisfies the given iterator.
*
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Replaces: UF_ATTR_ask_lock
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX11.0
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_user_attribute_lock
(
tag_t object, /* <I> The object holding the attribute */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attribute being queried.
The iterator is automatically reset. */
logical *is_locked, /* <O> The lock status of the set attribute or the template (if the attribute is unset) */
logical *has_attribute /* <O> An attribute or an unset template has been found*/
);
/****************************************************************************
* UF_ATTR_get_user_attribute
*
* Gets the information from the first attribute or template, if any, that satisfies the given iterator.
*
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attribute being queried.
The iterator is automatically reset. */
UF_ATTR_info_t *info, /* <OF> The attribute information for the first attribute (or unset template) found, if any.
This struct must be freed using UF_ATTR_free_user_attribute_info_strings() after use. */
logical *has_attribute /* <O> An attribute or an unset template has been found*/
);
/****************************************************************************
* UF_ATTR_get_null_user_attribute
*
* Queries the presence of a null type attribute
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_null_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
logical *has_attribute /* <O> An attribute has been found */
);
/****************************************************************************
* UF_ATTR_get_bool_user_attribute
*
* Gets value of a boolean type attribute, if it exists
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_bool_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
logical *value, /* <O> The value, if any */
logical *has_attribute /* <O> An attribute has been found */
);
/****************************************************************************
* UF_ATTR_get_integer_user_attribute
*
* Gets the value of a integer type attribute, if it exists
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_integer_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
int *value, /* <O> The value, if any */
logical *has_attribute /* <O> An attribute has been found */
);
/****************************************************************************
* UF_ATTR_get_real_user_attribute
*
* Gets the value and units of a real type attribute, if it exists
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_real_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
double *value, /* <O> The value, if any. If attribute has units, this value is in the returned units. */
tag_t *unit_type, /* <O> The unit type tag (NULL_TAG may be returned if unit-less) */
logical *has_attribute /* <O> An attribute has been found */
);
/****************************************************************************
* UF_ATTR_get_string_user_attribute
*
* Gets the value and reference string (if any) of a string type attribute, if it exists
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_string_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
char **string_value, /* <OF> String attribute value (Free using UF_free() after use) */
logical *has_attribute /* <O> An attribute has been found */
);
/****************************************************************************
* UF_ATTR_get_reference_string_of_user_attribute
*
* Gets the reference string (if any) of a string type attribute, if it exists and it has a reference string
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_reference_string_of_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
char **reference_string, /* <OF> Reference string (Free using UF_free() after use) */
logical *has_attribute /* <O> An attribute has been found AND it has a reference string */
);
/****************************************************************************
* UF_ATTR_get_computational_time_user_attribute
*
* Gets the value of a time type attribute, if it exists
* The returned time is in the local time of the program that is running.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_computational_time_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
int value[2], /* <O> Time/Date value as computational time */
logical *has_attribute /* <O> An attribute has been found */
);
/****************************************************************************
* UF_ATTR_get_string_time_user_attribute
*
* Gets the value of a time type attribute, if it exists
* The returned time is in the local time of the program that is running.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_string_time_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
const char *title, /* <I> The attribute title */
int index, /* <I> The array index (set to UF_ATTR_NOT_ARRAY if not an array) */
char **time_string, /* <OF> Time/Date value formatted as a string (Free using UF_free() after use) */
logical *has_attribute /* <O> An attribute has been found */
);
/****************************************************************************
* UF_ATTR_get_next_user_attribute
*
* Gets the information from the next attribute that satisfies the given iterator
*
* NOTE: If the iteration is allowed to completed, the iterator is automatically reset.
* If not, it must be reset with 'UF_ATTR_release_user_attribute_iterator()', or the iterator will leak memory.
* NOTE: The supplied 'info' struct must be initialized before use.
* Between calls to this function, the 'info' struct's strings do not have to be freed, as this is done prior to reading an attribute.
* However after the last call, the returned 'info' struct's strings must be freed.
* This can be done with UF_ATTR_free_user_attribute_info_strings().
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Replaces: UF_ATTR_cycle
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_next_user_attribute
(
tag_t object, /* <I> The object holding the attribute */
UF_ATTR_iterator_t *iter, /* <I/O> Iterator describing the attribute being queried.
If iteration is allowed to complete, iterator is reset by the system.
If not, reset with UF_ATTR_release_user_attribute_iterator() after use. */
UF_ATTR_info_t *info, /* <OF> The attribute information for the first attribute (or unset template) found, if any.
After iteration ends, free embedded strings using UF_ATTR_free_user_attribute_info_strings(). */
logical *has_attribute /* <O> An attribute (or unset template) has been found. If 'false', this ends the iteration. */
);
/****************************************************************************
* UF_ATTR_has_user_attribute_with_title_and_type
*
* Query the object for the existence of a set attribute that satisfies the given title and type.
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_has_user_attribute_with_title_and_type
(
tag_t object, /* <I> The object holding the attributes */
const char *title, /* <I> The title of the attribute */
int type, /* <I> The attribute type
Valid values:
UF_ATTR_integer
UF_ATTR_real
UF_ATTR_time
UF_ATTR_null
UF_ATTR_string
UF_ATTR_bool
UF_ATTR_any
NOTE: If UF_ATTR_any is used, the first attribute encountered that matches
the given title (and index), is noted as being present
*/
int index, /* <I> The array index ((set to UF_ATTR_NOT_ARRAY if not an array) */
logical *has_attribute /* <O> An attribute has been found */
);
/****************************************************************************
* UF_ATTR_has_user_attribute
*
* Query the object for the existence of an attribute that satisfies the given iterator
*
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_has_user_attribute
(
tag_t object, /* <I> The object holding the attributes */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attributes being queried.
The iterator is automatically reset. */
logical *has_attribute /* <O> An attribute (or unset template) has been found */
);
/****************************************************************************
* UF_ATTR_count_user_attributes
*
* Count the number of attributes that satisfy the given iterator.
*
* NOTE: This function counts individual array elements of arrays
* (in other words, an array with 'n' elements adds 'n' to the returned count.
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Replaces: UF_ATTR_count_attributes
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_count_user_attributes
(
tag_t object, /* <I> The object holding the attributes */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attributes being counted.
The iterator is automatically reset. */
int *count /* <O> The count of attributes (and/or unset templates) found */
);
/****************************************************************************
* UF_ATTR_count_user_attribute_titles
*
* Count the number of attributes that satisfy the given iterator
*
* NOTE: This function counts array attributes as one title.
* (in other words, an array with 'n' elements adds only one to the returned count.
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX10.0.0
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_count_user_attribute_titles
(
tag_t object, /* <I> The object holding the attributes */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attributes being counted.
The iterator is automatically reset. */
int *count /* <O> The count of attributes (and/or unset templates) found */
);
/****************************************************************************
* UF_ATTR_get_user_attributes
*
* Get information for all the attributes that satisfy the given iterator.
* This function will return an array of UF_ATTR_info_t structs that must be
* freed after use with UF_ATTR_free_user_attribute_info_array()
*
* Replaces: UF_ATTR_ask_part_attrs
* NOTE: No need to use UF_ATTR_ask_part_attribute() when reading part attributes. The part tag can be used.
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_user_attributes
(
tag_t object, /* <I> The object holding the attributes */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attributes being queried.
The iterator is automatically reset. */
int *num_attributes, /* <O> The number of attributes returned */
UF_ATTR_info_t **info /* <OF>
The information for the attributes (and/or unset templates) found.
Free using UF_ATTR_free_user_attribute_info_array() after use */
);
/****************************************************************************
* UF_ATTR_get_user_attributes_in_file
*
* Get information for all the part attributes in the given file that satisfy the given iterator.
* This function will return an array of UF_ATTR_info_t structs that must be
* freed after use with UF_ATTR_free_user_attribute_info_array()
*
* The given part file is temporarily partly opened to read the part attributes.
*
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* WARNING:
* * All values that have units will be returned in the attributes' current units.
* A string with the name of the units used is returned, but the unit tag is not.
* * Attribute expression references will not be returned.
* * All reference type attributes will be returned as plain string attributes.
* * The flags 'inherited', 'locked', 'required' are not returned by this function.
*
* Replaces: UF_ATTR_ask_part_attrs_in_file
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX11.0.0
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_get_user_attributes_in_file
(
const char *part_name, /* <I> The name of the part to be examined */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attributes being queried.
The iterator is automatically reset. */
int *num_attributes, /* <O> The number of attributes returned */
UF_ATTR_info_t **info /* <OF>
The information for the attributes (and/or unset templates) found.
Free using UF_ATTR_free_user_attribute_info_array() after use */
);
/****************************************************************************
* UF_ATTR_set_user_attribute_lock_with_title_and_type
*
* Set the locks of the the attributes that satisfy the given title and type
*
* Replaces: UF_ATTR_set_locked
*
*
* Environment: Internal and External
* See Also:
* History: NX11.0.0
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_user_attribute_lock_with_title_and_type
(
tag_t objectTag, /* <I> The object holding the attributes */
const char *title, /* <I> The title of the attribute */
int type, /* <I> The attribute type
Valid values:
UF_ATTR_integer
UF_ATTR_real
UF_ATTR_time
UF_ATTR_null
UF_ATTR_string
UF_ATTR_bool
UF_ATTR_any
NOTE: If UF_ATTR_any is used, the first attribute encountered that matches
the given title (and index), is deleted
*/
logical lock /* <I> The status of the lock to be set ('true': locked or 'false': unlocked) */
);
/****************************************************************************
* UF_ATTR_delete_user_attribute_with_title_and_type
*
* Delete the attribute with the given title and type
*
* Replaces: UF_ATTR_delete
*
* Replaces: UF_ATTR_set_locked
*
* Environment: Internal and External
* See Also:
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_delete_user_attribute_with_title_and_type
(
tag_t object, /* <I> The object holding the attributes */
const char *title, /* <I> The title of the attribute */
int type, /* <I> The attribute type
Valid values:
UF_ATTR_integer
UF_ATTR_real
UF_ATTR_time
UF_ATTR_null
UF_ATTR_string
UF_ATTR_bool
UF_ATTR_any
NOTE: If UF_ATTR_any is used, the first attribute encountered that matches
the given title (and index), is deleted
*/
int index, /* <I> The array index
Set to UF_ATTR_NOT_ARRAY if the attribute is not an array.
Set to UF_ATTR_LAST_ELEMENT if the attribute is an array.
*/
logical update /* <I> Perform an update immediately */
);
/****************************************************************************
* UF_ATTR_delete_user_attributes
*
* Delete all the attributes that satisfy the given iterator.
*
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Replaces: UF_ATTR_delete_all
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_delete_user_attributes
(
tag_t object, /* <I> The object holding the attributes */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attributes to be deleted.
The iterator is automatically reset. */
logical update /* <I> Perform an update immediately */
);
/****************************************************************************
* UF_ATTR_set_user_attribute_locks
*
* Set the locks on all the attributes that satisfy the given iterator.
*
* NOTE: This function cannot set locks on individual array elements
* NOTE: The UF_ATTR_iterator_t structure must be initialized using
* UF_ATTR_init_user_attribute_iterator before use.
*
* Environment: Internal and External
* See Also: UF_ATTR_init_user_attribute_iterator
* History: NX8.5.3
*****************************************************************************/
extern UFUNEXPORT int UF_ATTR_set_user_attribute_locks
(
tag_t object, /* <I> The object holding the attributes */
const UF_ATTR_iterator_t *iter, /* <I> Iterator describing the attributes to be locked.
The iterator is automatically reset. */
logical locked /* <I> The status of the lock to be set ('true': locked or 'false': unlocked) */
);
#undef EXPORTLIBRARY
#include <uf_retiring.h>
#endif /* UF_ATTR_INCLUDED */