UF_ASSEM_expl_status_e (view source)
Defined in: uf_assem.h
Also known as:
- UF_ASSEM_expl_status_t
- UF_ASSEM_expl_status_p_t
Data Members
UF_ASSEM_unexploded
UF_ASSEM_exploded
UF_ASSEM_revert_exploded
UF_ASSEM_level_option_e (view source)
Defined in: uf_assem_types.h
Also known as:
Overview
UF_ASSEM_level_option_t is used to control the results of an operation
to modify a part occurrence, when the part occurrence chosen
cannot be modified directly for some reason. It is currently
used for reposition.
Data Members
UF_ASSEM_use_strict_level
UF_ASSEM_use_existing_level
UF_ASSEM_establish_override
UF_ASSEM_part_load_option_e (view source)
Defined in: uf_assem_types.h
Also known as:
- UF_ASSEM_part_load_option_t
Overview
UF_ASSEM_part_load_option_t is used to control the part load option.
The first four settings are equivalent to the four possible
combinations of the partial loading and lightweight representations.
Data Members
UF_ASSEM_part_load_option_fully_load = 0
UF_ASSEM_part_load_option_partially_load = 1
UF_ASSEM_part_load_option_fully_load_lightweight_display = 2
UF_ASSEM_part_load_option_partially_load_lightweight_display = 3
UF_ASSEM_part_load_option_minimal_load_visualize = 4
UF_ASSEM_seq_playback_e (view source)
Defined in: uf_assem.h
Also known as:
- UF_ASSEM_seq_playback_t
- UF_ASSEM_seq_playback_p_t
Data Members
UF_ASSEM_seq_step_forward
UF_ASSEM_seq_step_backward
UF_ASSEM_seq_play_forward
UF_ASSEM_seq_play_backward