UF_ABORT_ask_flag_status (view source)
Defined in: uf_abort.h
Overview
This routine is used to check whether the user has signaled an abort request
by pressing the key sequence CTRL+SHIFT+L or selecting OK in the Work
In Progress dialog if NX has not had a chance to act on the signal.
But if NX has already processed the abort request by the time this function
is called, then the return code is FALSE as the abort signal is already reset.
Return
Return code = 0 : successful
> 0 : failing error number
< 0 : failing error number
Environment
Internal and External
History
Introduced in V16.0.3
Required License(s)
gateway
int UF_ABORT_ask_flag_status
(
logical * flag
)
logical * | flag | Output | when set to TRUE, indicates an abort signal |
UF_ABORT_clear_abort (view source)
Defined in: uf_abort.h
Overview
This routine is used to clear any pending abort requests. It should be
called if the abort request is handled.
Return
Return code = 0 : successful
> 0 : failing error number
< 0 : failing error number
Environment
Internal and External
History
Introduced in V16.0.3
Required License(s)
gateway
int UF_ABORT_clear_abort
(
void
)
UF_ABORT_disable_abort (view source)
Defined in: uf_abort.h
Overview
This routine is used to disable the abort handler. It must be re-enabled with
the function, UF_ABORT_enable_abort.
Return
Return code = 0 : successful
> 0 : failing error number
< 0 : failing error number
Environment
Internal and External
History
Introduced in V18.0
Required License(s)
gateway
int UF_ABORT_disable_abort
(
void
)
UF_ABORT_enable_abort (view source)
Defined in: uf_abort.h
Overview
This routine is used to enable the abort handler. It is used in conjunction
with UF_ABORT_disable_abort.
Return
Return code = 0 : successful
> 0 : failing error number
< 0 : failing error number
Environment
Internal and External
History
Introduced in V18.0
Required License(s)
gateway
int UF_ABORT_enable_abort
(
void
)