public interface WeldPointExitBuilder extends TaggedObject, IComponentBuilder
WeldPointExitBuilder
class used to pass welding object from the Weld Point command to a user callback. This object is not used on edit.
Modifier and Type | Interface and Description |
---|---|
static class |
WeldPointExitBuilder.CommandName
The command name used for the newly created features.
|
static class |
WeldPointExitBuilder.FeatureInfo
Structure used to identify newly created features.
|
static class |
WeldPointExitBuilder.MethodUsed
The method use to create the features.
|
Modifier and Type | Method and Description |
---|---|
WeldPointExitBuilder.CommandName |
commandUsed()
Returns the command name that was last used to create features.
|
WeldPointExitBuilder.FeatureInfo[] |
getFeatureInformation()
Gets the information for the newly created features.
|
printTestData, printTestData, tag, tagValue
validate
WeldPointExitBuilder.CommandName commandUsed() throws NXException, RemoteException
NXException
RemoteException
WeldPointExitBuilder.FeatureInfo[] getFeatureInformation() throws NXException, RemoteException
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.