public class WeldPointDirection extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END_TO_START
Direction is from end to start
|
static int |
_START_TO_END
Direction is from start to end
|
static WeldPointDirection |
END_TO_START
Direction is from end to start
|
static WeldPointDirection |
START_TO_END
Direction is from start to end
|
Modifier and Type | Method and Description |
---|---|
static WeldPointDirection |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPointDirection |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPointDirection[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldPointDirection START_TO_END
public static final WeldPointDirection END_TO_START
public static final int _START_TO_END
public static final int _END_TO_START
public static WeldPointDirection valueOf(int value)
public static WeldPointDirection valueOf(String name)
public static WeldPointDirection[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.