public interface ExportWeldJointBuilder extends ExportWeldBuilder
WeldManager.createExportWeldJointBuilder()
Property | Value |
---|---|
AttributeOrigin | Object |
ChordalTolerance.Value | 2.54 (millimeters part), 0.1 (inches part) |
Output | IntermediateFile |
ExportWeldBuilder.AttributeOriginType, ExportWeldBuilder.OutputType
Modifier and Type | Method and Description |
---|---|
Expression |
chordalTolerance()
Returns the minimum chordal length used to create a discrete version of the weld path, points along it will be output into
xml file to represent the weld path
License requirements: None. |
boolean |
outputFilletFaceInfo()
Returns the indication to output face normals at each point if leg lengths are defined.
|
void |
setOutputFilletFaceInfo(boolean status)
License requirements: structure_weld ("STRUCTURE WELD") . |
void |
setWorkCoordinateSystem(CoordinateSystem coordSystem)
License requirements: structure_weld ("STRUCTURE WELD") . |
CoordinateSystem |
workCoordinateSystem()
Returns the local coordinate system used to calculate the output points on welding joint.
|
attributeOrigin, connectedPartAttrToggle, csvFileName, getConnectedPartAttributes, getExportedAttributes, openFromFile, output, readAttributesFromWelds, restoreDefault, saveAsDefault, saveToFile, setAttributeOrigin, setConnectedPartAttributes, setConnectedPartAttrToggle, setCsvFileName, setExportedAttributes, setOutput, setTemplateFileName, templateFileName, weldPoints
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
CoordinateSystem workCoordinateSystem() throws NXException, RemoteException
NXException
RemoteException
void setWorkCoordinateSystem(CoordinateSystem coordSystem) throws NXException, RemoteException
coordSystem
- NXException
RemoteException
Expression chordalTolerance() throws NXException, RemoteException
NXException
RemoteException
boolean outputFilletFaceInfo() throws NXException, RemoteException
NXException
RemoteException
void setOutputFilletFaceInfo(boolean status) throws NXException, RemoteException
status
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.