public static class SpecialPiercingInsertBuilder.ParentPartTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PROJECT_DIE |
static int |
_PROJECT_DIE_BASE |
static int |
_PROJECT_SUB_DIE_BASE |
static SpecialPiercingInsertBuilder.ParentPartTypes |
PROJECT_DIE |
static SpecialPiercingInsertBuilder.ParentPartTypes |
PROJECT_DIE_BASE |
static SpecialPiercingInsertBuilder.ParentPartTypes |
PROJECT_SUB_DIE_BASE |
Modifier and Type | Method and Description |
---|---|
static SpecialPiercingInsertBuilder.ParentPartTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpecialPiercingInsertBuilder.ParentPartTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpecialPiercingInsertBuilder.ParentPartTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final SpecialPiercingInsertBuilder.ParentPartTypes PROJECT_DIE
public static final SpecialPiercingInsertBuilder.ParentPartTypes PROJECT_DIE_BASE
public static final SpecialPiercingInsertBuilder.ParentPartTypes PROJECT_SUB_DIE_BASE
public static final int _PROJECT_DIE
public static final int _PROJECT_DIE_BASE
public static final int _PROJECT_SUB_DIE_BASE
public static SpecialPiercingInsertBuilder.ParentPartTypes valueOf(int value)
public static SpecialPiercingInsertBuilder.ParentPartTypes valueOf(String name)
public static SpecialPiercingInsertBuilder.ParentPartTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.