public static class PiercingInsertBuilder.PunchPocketTypeItemsBP extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CIRCLE
Punch pocket type in backing plate is circle
|
static int |
_CLEARANCE
Punch pocket type in backing plate is clearance
|
static int |
_FILLET
Punch pocket type in backing plate is fillet
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
CIRCLE
Punch pocket type in backing plate is circle
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
CLEARANCE
Punch pocket type in backing plate is clearance
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
FILLET
Punch pocket type in backing plate is fillet
|
Modifier and Type | Method and Description |
---|---|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP[] |
values()
Returns an array that contains the values for this enum.
|
public static final PiercingInsertBuilder.PunchPocketTypeItemsBP CLEARANCE
public static final PiercingInsertBuilder.PunchPocketTypeItemsBP FILLET
public static final PiercingInsertBuilder.PunchPocketTypeItemsBP CIRCLE
public static final int _CLEARANCE
public static final int _FILLET
public static final int _CIRCLE
public static PiercingInsertBuilder.PunchPocketTypeItemsBP valueOf(int value)
public static PiercingInsertBuilder.PunchPocketTypeItemsBP valueOf(String name)
public static PiercingInsertBuilder.PunchPocketTypeItemsBP[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.