public static class PiercingInsertBuilder.AssociationToolType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADD_INTO_LIST
The operation option is add into list
|
static int |
_DELETE_SELECTED_INSERTS
The operation option is delete selected inserts
|
static int |
_REMOVE_FROM_LIST
The operation option is remove from list
|
static PiercingInsertBuilder.AssociationToolType |
ADD_INTO_LIST
The operation option is add into list
|
static PiercingInsertBuilder.AssociationToolType |
DELETE_SELECTED_INSERTS
The operation option is delete selected inserts
|
static PiercingInsertBuilder.AssociationToolType |
REMOVE_FROM_LIST
The operation option is remove from list
|
Modifier and Type | Method and Description |
---|---|
static PiercingInsertBuilder.AssociationToolType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PiercingInsertBuilder.AssociationToolType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PiercingInsertBuilder.AssociationToolType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PiercingInsertBuilder.AssociationToolType ADD_INTO_LIST
public static final PiercingInsertBuilder.AssociationToolType REMOVE_FROM_LIST
public static final PiercingInsertBuilder.AssociationToolType DELETE_SELECTED_INSERTS
public static final int _ADD_INTO_LIST
public static final int _REMOVE_FROM_LIST
public static final int _DELETE_SELECTED_INSERTS
public static PiercingInsertBuilder.AssociationToolType valueOf(int value)
public static PiercingInsertBuilder.AssociationToolType valueOf(String name)
public static PiercingInsertBuilder.AssociationToolType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.