public static class LsdynaFormAnalysisResultDisplayBuilder.StressTypeName extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAXIMUM_INPLANE_STRESS
Display maximum in-plane stress.
|
static int |
_MINIMUM_INPLANE_STRESS
Display minimum in-plane stress.
|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
MAXIMUM_INPLANE_STRESS
Display maximum in-plane stress.
|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
MINIMUM_INPLANE_STRESS
Display minimum in-plane stress.
|
Modifier and Type | Method and Description |
---|---|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName[] |
values()
Returns an array that contains the values for this enum.
|
public static final LsdynaFormAnalysisResultDisplayBuilder.StressTypeName MAXIMUM_INPLANE_STRESS
public static final LsdynaFormAnalysisResultDisplayBuilder.StressTypeName MINIMUM_INPLANE_STRESS
public static final int _MAXIMUM_INPLANE_STRESS
public static final int _MINIMUM_INPLANE_STRESS
public static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName valueOf(int value)
public static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName valueOf(String name)
public static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.