public static class ForceCalculationBuilder.CalculationTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ISOLATED
calculate force in isolation, without considering other processes
|
static int |
_NORMAL
calculate force considering pre-stations effects
|
static ForceCalculationBuilder.CalculationTypes |
ISOLATED
calculate force in isolation, without considering other processes
|
static ForceCalculationBuilder.CalculationTypes |
NORMAL
calculate force considering pre-stations effects
|
Modifier and Type | Method and Description |
---|---|
static ForceCalculationBuilder.CalculationTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ForceCalculationBuilder.CalculationTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ForceCalculationBuilder.CalculationTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ForceCalculationBuilder.CalculationTypes NORMAL
public static final ForceCalculationBuilder.CalculationTypes ISOLATED
public static final int _NORMAL
public static final int _ISOLATED
public static ForceCalculationBuilder.CalculationTypes valueOf(int value)
public static ForceCalculationBuilder.CalculationTypes valueOf(String name)
public static ForceCalculationBuilder.CalculationTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.