public static class DieCavityAndSlugHoleBuilder.DieInsertStackType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE |
static int |
_THREE |
static int |
_TWO |
static DieCavityAndSlugHoleBuilder.DieInsertStackType |
ONE |
static DieCavityAndSlugHoleBuilder.DieInsertStackType |
THREE |
static DieCavityAndSlugHoleBuilder.DieInsertStackType |
TWO |
Modifier and Type | Method and Description |
---|---|
static DieCavityAndSlugHoleBuilder.DieInsertStackType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieCavityAndSlugHoleBuilder.DieInsertStackType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieCavityAndSlugHoleBuilder.DieInsertStackType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DieCavityAndSlugHoleBuilder.DieInsertStackType ONE
public static final DieCavityAndSlugHoleBuilder.DieInsertStackType TWO
public static final DieCavityAndSlugHoleBuilder.DieInsertStackType THREE
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static DieCavityAndSlugHoleBuilder.DieInsertStackType valueOf(int value)
public static DieCavityAndSlugHoleBuilder.DieInsertStackType valueOf(String name)
public static DieCavityAndSlugHoleBuilder.DieInsertStackType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.