public static class AutoDimensionBuilder.TextOrientationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALIGNED |
static int |
_HORIZONTAL |
static int |
_PERPENDICULAR |
static int |
_TEXT_AT_ANGLE |
static int |
_TEXT_OVER_DIMENSION_LINE |
static AutoDimensionBuilder.TextOrientationType |
ALIGNED |
static AutoDimensionBuilder.TextOrientationType |
HORIZONTAL |
static AutoDimensionBuilder.TextOrientationType |
PERPENDICULAR |
static AutoDimensionBuilder.TextOrientationType |
TEXT_AT_ANGLE |
static AutoDimensionBuilder.TextOrientationType |
TEXT_OVER_DIMENSION_LINE |
Modifier and Type | Method and Description |
---|---|
static AutoDimensionBuilder.TextOrientationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AutoDimensionBuilder.TextOrientationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AutoDimensionBuilder.TextOrientationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AutoDimensionBuilder.TextOrientationType HORIZONTAL
public static final AutoDimensionBuilder.TextOrientationType ALIGNED
public static final AutoDimensionBuilder.TextOrientationType TEXT_OVER_DIMENSION_LINE
public static final AutoDimensionBuilder.TextOrientationType TEXT_AT_ANGLE
public static final AutoDimensionBuilder.TextOrientationType PERPENDICULAR
public static final int _HORIZONTAL
public static final int _ALIGNED
public static final int _TEXT_OVER_DIMENSION_LINE
public static final int _TEXT_AT_ANGLE
public static final int _PERPENDICULAR
public static AutoDimensionBuilder.TextOrientationType valueOf(int value)
public static AutoDimensionBuilder.TextOrientationType valueOf(String name)
public static AutoDimensionBuilder.TextOrientationType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.