public interface KinematicImportMcfBuilder extends Builder
Part
class to create a KinematicImportMcfBuilder object. Modifier and Type | Method and Description |
---|---|
boolean |
ignoreLimits()
Returns the flag which determines if the Limits of the MCF and the Kim are merge.
|
String |
mcfPath()
Returns the path from the mcf file
License requirements: None. |
boolean |
replaceChannel()
Returns the flag which determines if the channel data of the Machine Tool Builder are
deleted befor they are replaced through the Channel data of the MCF-File
License requirements: None. |
void |
setIgnoreLimits(boolean replace)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
void |
setMcfPath(String path)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
void |
setReplaceChannel(boolean replace)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
String mcfPath() throws NXException, RemoteException
NXException
RemoteException
void setMcfPath(String path) throws NXException, RemoteException
path
- The MCF PathNXException
RemoteException
boolean replaceChannel() throws NXException, RemoteException
NXException
RemoteException
void setReplaceChannel(boolean replace) throws NXException, RemoteException
replace
- NXException
RemoteException
boolean ignoreLimits() throws NXException, RemoteException
NXException
RemoteException
void setIgnoreLimits(boolean replace) throws NXException, RemoteException
replace
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.