public static class SplinePathBuilder.DragMode extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ACTIVE
The drag network is active
|
static int |
_INACTIVE
The drag network is inactive
|
static SplinePathBuilder.DragMode |
ACTIVE
The drag network is active
|
static SplinePathBuilder.DragMode |
INACTIVE
The drag network is inactive
|
Modifier and Type | Method and Description |
---|---|
static SplinePathBuilder.DragMode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplinePathBuilder.DragMode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplinePathBuilder.DragMode[] |
values()
Returns an array that contains the values for this enum.
|
public static final SplinePathBuilder.DragMode ACTIVE
public static final SplinePathBuilder.DragMode INACTIVE
public static final int _ACTIVE
public static final int _INACTIVE
public static SplinePathBuilder.DragMode valueOf(int value)
public static SplinePathBuilder.DragMode valueOf(String name)
public static SplinePathBuilder.DragMode[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.