public static class SplinePathBuilder.DefiningPointMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CREATE_POINT |
static int |
_USE_EXISTING |
static SplinePathBuilder.DefiningPointMethod |
CREATE_POINT |
static SplinePathBuilder.DefiningPointMethod |
USE_EXISTING |
Modifier and Type | Method and Description |
---|---|
static SplinePathBuilder.DefiningPointMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplinePathBuilder.DefiningPointMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplinePathBuilder.DefiningPointMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final SplinePathBuilder.DefiningPointMethod CREATE_POINT
public static final SplinePathBuilder.DefiningPointMethod USE_EXISTING
public static final int _CREATE_POINT
public static final int _USE_EXISTING
public static SplinePathBuilder.DefiningPointMethod valueOf(int value)
public static SplinePathBuilder.DefiningPointMethod valueOf(String name)
public static SplinePathBuilder.DefiningPointMethod[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.