public static class Run.FlipStatus extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CANNOT_FLIP
Run is deleted or there are no segments attached to component.
|
static int |
_FLOW_TYPE_MISMATCH
Ports are defined with ambiguous flow types.
|
static int |
_FOLLOWS_FLOW
Ports correctly aligned with flow.
|
static int |
_NOT_TWO_PORTS
Given component ports are not equal to two ports.
|
static int |
_PORT_POSITION_MISMATCH
Ports are not collinear and opposite or perpendicular.
|
static int |
_RUN_FLOW_NOT_DEFINED
Flow is not defined on Run.
|
static int |
_SUCCESS
Component is flipped.
|
static int |
_UNEQUAL_CONSTRAINTS
Each ports has different number of constraints.
|
static Run.FlipStatus |
CANNOT_FLIP
Run is deleted or there are no segments attached to component.
|
static Run.FlipStatus |
FLOW_TYPE_MISMATCH
Ports are defined with ambiguous flow types.
|
static Run.FlipStatus |
FOLLOWS_FLOW
Ports correctly aligned with flow.
|
static Run.FlipStatus |
NOT_TWO_PORTS
Given component ports are not equal to two ports.
|
static Run.FlipStatus |
PORT_POSITION_MISMATCH
Ports are not collinear and opposite or perpendicular.
|
static Run.FlipStatus |
RUN_FLOW_NOT_DEFINED
Flow is not defined on Run.
|
static Run.FlipStatus |
SUCCESS
Component is flipped.
|
static Run.FlipStatus |
UNEQUAL_CONSTRAINTS
Each ports has different number of constraints.
|
Modifier and Type | Method and Description |
---|---|
static Run.FlipStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Run.FlipStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Run.FlipStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final Run.FlipStatus SUCCESS
public static final Run.FlipStatus NOT_TWO_PORTS
public static final Run.FlipStatus UNEQUAL_CONSTRAINTS
public static final Run.FlipStatus PORT_POSITION_MISMATCH
public static final Run.FlipStatus FLOW_TYPE_MISMATCH
public static final Run.FlipStatus FOLLOWS_FLOW
public static final Run.FlipStatus RUN_FLOW_NOT_DEFINED
public static final Run.FlipStatus CANNOT_FLIP
public static final int _SUCCESS
public static final int _NOT_TWO_PORTS
public static final int _UNEQUAL_CONSTRAINTS
public static final int _PORT_POSITION_MISMATCH
public static final int _FLOW_TYPE_MISMATCH
public static final int _FOLLOWS_FLOW
public static final int _RUN_FLOW_NOT_DEFINED
public static final int _CANNOT_FLIP
public static Run.FlipStatus valueOf(int value)
public static Run.FlipStatus valueOf(String name)
public static Run.FlipStatus[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.