public class ProfileFrom extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
Profile is at the end of the last segment.
|
static int |
_START
Profile is at the start of the first segment.
|
static ProfileFrom |
END
Profile is at the end of the last segment.
|
static ProfileFrom |
START
Profile is at the start of the first segment.
|
Modifier and Type | Method and Description |
---|---|
static ProfileFrom |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProfileFrom |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProfileFrom[] |
values()
Returns an array that contains the values for this enum.
|
public static final ProfileFrom START
public static final ProfileFrom END
public static final int _START
public static final int _END
public static ProfileFrom valueOf(int value)
public static ProfileFrom valueOf(String name)
public static ProfileFrom[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.