public class PointDefinition extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
The point defines the end of the overstock application.
|
static int |
_MIDDLE
The point defines the middle of the overstock application.
|
static int |
_START
The point defines the start of the overstock application.
|
static PointDefinition |
END
The point defines the end of the overstock application.
|
static PointDefinition |
MIDDLE
The point defines the middle of the overstock application.
|
static PointDefinition |
START
The point defines the start of the overstock application.
|
Modifier and Type | Method and Description |
---|---|
static PointDefinition |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointDefinition |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointDefinition[] |
values()
Returns an array that contains the values for this enum.
|
public static final PointDefinition START
public static final PointDefinition MIDDLE
public static final PointDefinition END
public static final int _START
public static final int _MIDDLE
public static final int _END
public static PointDefinition valueOf(int value)
public static PointDefinition valueOf(String name)
public static PointDefinition[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.