public static class DesignRuleViolationLocationCollection.DeleteOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DO_DELETE |
static int |
_DONT_DELETE
Set this option only if you do not want to delete violation location objects
|
static DesignRuleViolationLocationCollection.DeleteOption |
DO_DELETE |
static DesignRuleViolationLocationCollection.DeleteOption |
DONT_DELETE
Set this option only if you do not want to delete violation location objects
|
Modifier and Type | Method and Description |
---|---|
static DesignRuleViolationLocationCollection.DeleteOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DesignRuleViolationLocationCollection.DeleteOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DesignRuleViolationLocationCollection.DeleteOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final DesignRuleViolationLocationCollection.DeleteOption DO_DELETE
public static final DesignRuleViolationLocationCollection.DeleteOption DONT_DELETE
public static final int _DO_DELETE
public static final int _DONT_DELETE
public static DesignRuleViolationLocationCollection.DeleteOption valueOf(int value)
public static DesignRuleViolationLocationCollection.DeleteOption valueOf(String name)
public static DesignRuleViolationLocationCollection.DeleteOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.