public interface ConnectPathBuilder extends Builder
ConnectPathBuilder
.
Routing.ConnectPathBuilderis used to control the connecting of
Routing.ControlPoints within the distance tolerance specified.
This eliminates duplicate Routing.ControlPoints such that only one
Routing.ControlPoint remains. The Routing.Segments that were defined
by the duplicate Routing.ControlPoints are now defined by the remaining
Routing.ControlPoint. Routing.ConnectPath is the reverse operation to
Routing.DiscontinuityCorner. RouteManager.createConnectPathBuilder()
Property | Value |
---|---|
Tolerance | 0.01 (millimeters part), 0.001 (inches part) |
Modifier and Type | Method and Description |
---|---|
SelectNXObjectList |
selection()
Returns the Routing.ControlPoints that are selected.
|
void |
setTolerance(double tolerance)
License requirements: routing_base ("Routing Basic") . |
double |
tolerance()
Returns the 3D distance within which Routing.ControlPoints will be considered duplicates
and some will be merged away so that only one Routing.ControlPoint remains.
|
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectNXObjectList selection() throws NXException, RemoteException
NXException
RemoteException
double tolerance() throws NXException, RemoteException
NXException
RemoteException
void setTolerance(double tolerance) throws NXException, RemoteException
tolerance
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.