public interface AnchorCollection extends TaggedObjectCollection
Anchor
objects.
Iterating this collection only returns live uncondemned objects contained in the owning part
of the collection. Note that Anchor
is a smart object and many smart objects are condemned as they
only exist to support other objects and are not displayed. RouteManager
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
Anchor |
createAnchor(Point3d origin)
Creates a
Anchor object. |
Anchor |
createAnchor(Point3d position,
Point point)
Creates a
Anchor object. |
_find_next, iterator
Anchor createAnchor(Point3d origin) throws NXException, RemoteException
Anchor
object.
origin
- Origin of the AnchorNXException
RemoteException
Anchor createAnchor(Point3d position, Point point) throws NXException, RemoteException
Anchor
object.
position
- This can be nullpoint
- Anchor to this. If this is null use positionNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.