public static class SketchPreferences.DimensionLabelType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXPRESSION
Displays the entire expression such as P2=P3*4
|
static int |
_NAME
Displays only the name of the expression, such as P2
|
static int |
_VALUE
Displays the numerical value of the expression
|
static SketchPreferences.DimensionLabelType |
EXPRESSION
Displays the entire expression such as P2=P3*4
|
static SketchPreferences.DimensionLabelType |
NAME
Displays only the name of the expression, such as P2
|
static SketchPreferences.DimensionLabelType |
VALUE
Displays the numerical value of the expression
|
Modifier and Type | Method and Description |
---|---|
static SketchPreferences.DimensionLabelType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchPreferences.DimensionLabelType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchPreferences.DimensionLabelType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SketchPreferences.DimensionLabelType EXPRESSION
public static final SketchPreferences.DimensionLabelType NAME
public static final SketchPreferences.DimensionLabelType VALUE
public static final int _EXPRESSION
public static final int _NAME
public static final int _VALUE
public static SketchPreferences.DimensionLabelType valueOf(int value)
public static SketchPreferences.DimensionLabelType valueOf(String name)
public static SketchPreferences.DimensionLabelType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.