public static class SessionModeling.SketchDefaultActionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EDIT
Edit sketch without rollback on double click
|
static int |
_EDIT_WITH_ROLLBACK
Edit sketch with rollback on double click
|
static SessionModeling.SketchDefaultActionType |
EDIT
Edit sketch without rollback on double click
|
static SessionModeling.SketchDefaultActionType |
EDIT_WITH_ROLLBACK
Edit sketch with rollback on double click
|
Modifier and Type | Method and Description |
---|---|
static SessionModeling.SketchDefaultActionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.SketchDefaultActionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.SketchDefaultActionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionModeling.SketchDefaultActionType EDIT_WITH_ROLLBACK
public static final SessionModeling.SketchDefaultActionType EDIT
public static final int _EDIT_WITH_ROLLBACK
public static final int _EDIT
public static SessionModeling.SketchDefaultActionType valueOf(int value)
public static SessionModeling.SketchDefaultActionType valueOf(String name)
public static SessionModeling.SketchDefaultActionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.