public static class RoutingMechanical.LineColorType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HEX |
static int |
_INDEX |
static int |
_MAX |
static int |
_NAME |
static int |
_RGB |
static int |
_UNKNOWN |
static RoutingMechanical.LineColorType |
HEX |
static RoutingMechanical.LineColorType |
INDEX |
static RoutingMechanical.LineColorType |
MAX |
static RoutingMechanical.LineColorType |
NAME |
static RoutingMechanical.LineColorType |
RGB |
static RoutingMechanical.LineColorType |
UNKNOWN |
Modifier and Type | Method and Description |
---|---|
static RoutingMechanical.LineColorType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingMechanical.LineColorType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingMechanical.LineColorType[] |
values()
Returns an array that contains the values for this enum.
|
public static final RoutingMechanical.LineColorType UNKNOWN
public static final RoutingMechanical.LineColorType NAME
public static final RoutingMechanical.LineColorType INDEX
public static final RoutingMechanical.LineColorType RGB
public static final RoutingMechanical.LineColorType HEX
public static final RoutingMechanical.LineColorType MAX
public static final int _UNKNOWN
public static final int _NAME
public static final int _INDEX
public static final int _RGB
public static final int _HEX
public static final int _MAX
public static RoutingMechanical.LineColorType valueOf(int value)
public static RoutingMechanical.LineColorType valueOf(String name)
public static RoutingMechanical.LineColorType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.