public class GdtOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FROM_MODEL_VIEW
inherit display instances of geometric tolerance features that exist in a particular modeling view (e.g.
|
static int |
_IN_DRAWING_PLANE
inherit display instances of geometric tolerance features that are parallel to the drawing plane onto the drawing view.
|
static int |
_NONE
Does not inherit any GD and T display instances.
|
static GdtOption |
FROM_MODEL_VIEW
inherit display instances of geometric tolerance features that exist in a particular modeling view (e.g.
|
static GdtOption |
IN_DRAWING_PLANE
inherit display instances of geometric tolerance features that are parallel to the drawing plane onto the drawing view.
|
static GdtOption |
NONE
Does not inherit any GD and T display instances.
|
Modifier and Type | Method and Description |
---|---|
static GdtOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GdtOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GdtOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final GdtOption NONE
public static final GdtOption IN_DRAWING_PLANE
public static final GdtOption FROM_MODEL_VIEW
public static final int _NONE
public static final int _IN_DRAWING_PLANE
public static final int _FROM_MODEL_VIEW
public static GdtOption valueOf(int value)
public static GdtOption valueOf(String name)
public static GdtOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.