public interface BaseViewPreferences extends IBaseViewPreferences
ViewPreferences.baseView()
Modifier and Type | Method and Description |
---|---|
void |
setFacetedRepresentation(boolean isFacetedRepresentation)
Deprecated.
Deprecated in NX8.5.1. Use
GeneralViewPreferences.setViewRepresentation(nxopen.preferences.GeneralViewRepresentationOption) instead.
|
void |
setInheritClippingBoundary(boolean isInheritClippingBoundary)
The status of inherit clipping boundary, if True the model view's
clipping boundary are inherited when model view is imported onto the drawing, else
the imported model view is placed on the drawing with an Automatic Rectangular Boundary.
|
void |
setTransferAnnotation(boolean isTransferAnnotation)
The status of transfer annotation controls whether or not annotations created in
a model view are transferred to the drawing when a view is imported.
|
void setFacetedRepresentation(boolean isFacetedRepresentation) throws NXException, RemoteException
GeneralViewPreferences.setViewRepresentation(nxopen.preferences.GeneralViewRepresentationOption)
instead.
isFacetedRepresentation
- NXException
RemoteException
void setInheritClippingBoundary(boolean isInheritClippingBoundary) throws NXException, RemoteException
isInheritClippingBoundary
- Inherit XY clipping boundaries of modelNXException
RemoteException
void setTransferAnnotation(boolean isTransferAnnotation) throws NXException, RemoteException
isTransferAnnotation
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.