public static class ComponentConstraintGroup.ConstraintsCollectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BETWEEN_SELECTED_COMPONENTS |
static int |
_CONNECTED_TO_SELECTED_COMPONENTS |
static ComponentConstraintGroup.ConstraintsCollectionType |
BETWEEN_SELECTED_COMPONENTS |
static ComponentConstraintGroup.ConstraintsCollectionType |
CONNECTED_TO_SELECTED_COMPONENTS |
Modifier and Type | Method and Description |
---|---|
static ComponentConstraintGroup.ConstraintsCollectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComponentConstraintGroup.ConstraintsCollectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComponentConstraintGroup.ConstraintsCollectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ComponentConstraintGroup.ConstraintsCollectionType BETWEEN_SELECTED_COMPONENTS
public static final ComponentConstraintGroup.ConstraintsCollectionType CONNECTED_TO_SELECTED_COMPONENTS
public static final int _BETWEEN_SELECTED_COMPONENTS
public static final int _CONNECTED_TO_SELECTED_COMPONENTS
public static ComponentConstraintGroup.ConstraintsCollectionType valueOf(int value)
public static ComponentConstraintGroup.ConstraintsCollectionType valueOf(String name)
public static ComponentConstraintGroup.ConstraintsCollectionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.