public static class TableDocumentData.CaptionPosition extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ABOVE
the above position
|
static int |
_BELLOW
the bellow position
|
static TableDocumentData.CaptionPosition |
ABOVE
the above position
|
static TableDocumentData.CaptionPosition |
BELLOW
the bellow position
|
Modifier and Type | Method and Description |
---|---|
static TableDocumentData.CaptionPosition |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TableDocumentData.CaptionPosition |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TableDocumentData.CaptionPosition[] |
values()
Returns an array that contains the values for this enum.
|
public static final TableDocumentData.CaptionPosition ABOVE
public static final TableDocumentData.CaptionPosition BELLOW
public static final int _ABOVE
public static final int _BELLOW
public static TableDocumentData.CaptionPosition valueOf(int value)
public static TableDocumentData.CaptionPosition valueOf(String name)
public static TableDocumentData.CaptionPosition[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.