public static class TextBasedElementBuilder.TypeChoices extends Enum
Modifier and Type | Method and Description |
---|---|
static TextBasedElementBuilder.TypeChoices |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TextBasedElementBuilder.TypeChoices |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TextBasedElementBuilder.TypeChoices[] |
values()
Returns an array that contains the values for this enum.
|
public static final TextBasedElementBuilder.TypeChoices THREE_POINT_FORCE
public static final TextBasedElementBuilder.TypeChoices THREE_POINT_TORQUE
public static final TextBasedElementBuilder.TypeChoices ALL_KINEMATIC_DIRECTION_SENSOR
public static final TextBasedElementBuilder.TypeChoices ALL_FORCE_DIRECTION_SENSOR
public static final TextBasedElementBuilder.TypeChoices AERO_AERO_FORCE
public static final TextBasedElementBuilder.TypeChoices AERO_HYDRO_FORCE
public static final TextBasedElementBuilder.TypeChoices AERO_VEHICLE_FORCE
public static final TextBasedElementBuilder.TypeChoices CUSTOMIZED_SOLVER
public static final TextBasedElementBuilder.TypeChoices STI_TIRE
public static final TextBasedElementBuilder.TypeChoices STI_TIRE_PROPERTY
public static final TextBasedElementBuilder.TypeChoices BUMP_STOP_CONTACT
public static final TextBasedElementBuilder.TypeChoices SPHERE_TO_GROUND_CONTACT
public static final TextBasedElementBuilder.TypeChoices GEAR_CONTACT
public static final TextBasedElementBuilder.TypeChoices THREE_LINK_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices FOUR_LINK_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices FIVE_LINK_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices ROLL_IAX_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices STEER_IAX_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices HOTCH_KISS_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices MC_PHERSON_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices DOUBLE_AARM_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices PIVOT_BEAM_SUSPENSION
public static final TextBasedElementBuilder.TypeChoices VEHICLE
public static final TextBasedElementBuilder.TypeChoices SPEED_SWEEP
public static final TextBasedElementBuilder.TypeChoices SYSTEM_PROPERTY
public static final TextBasedElementBuilder.TypeChoices DYNAMIC_PROPERTY
public static final TextBasedElementBuilder.TypeChoices KINEMATIC_PROPERTY
public static final TextBasedElementBuilder.TypeChoices STATIC_PROPERTY
public static final TextBasedElementBuilder.TypeChoices PRELOAD_PROPERTY
public static final TextBasedElementBuilder.TypeChoices INVERSE_PROPERTY
public static final TextBasedElementBuilder.TypeChoices LINEARIZATION_PROPERTY
public static final TextBasedElementBuilder.TypeChoices RESTART_PROPERTY
public static final TextBasedElementBuilder.TypeChoices ADVANCED_SOLUTION
public static final TextBasedElementBuilder.TypeChoices GEAR
public static final TextBasedElementBuilder.TypeChoices GENERIC
public static final TextBasedElementBuilder.TypeChoices FMI
public static final TextBasedElementBuilder.TypeChoices POINT_TO_POINT_CONSTRAINT
public static final TextBasedElementBuilder.TypeChoices ORIENTATION_CONSTRAINT
public static final TextBasedElementBuilder.TypeChoices FUNCTIONCURVE_CONTROL_INPUT
public static final TextBasedElementBuilder.TypeChoices PATH_FOLLOWER_CONTROL_INPUT
public static final TextBasedElementBuilder.TypeChoices USER_DEFINED_CONTROL_INPUT
public static final TextBasedElementBuilder.TypeChoices SPECIAL_CONTROL_INPUT
public static final TextBasedElementBuilder.TypeChoices LINEAR_CONTROL_OUTPUT
public static final TextBasedElementBuilder.TypeChoices MASS_PROPERTY_CONTROL_OUTPUT
public static final TextBasedElementBuilder.TypeChoices LINK_INITIAL_CONDITION
public static final TextBasedElementBuilder.TypeChoices SCREW_JOINT_OR_SPRING_INITIAL_CONDITION
public static final TextBasedElementBuilder.TypeChoices FLEXIBLE_LINK_INITIAL_CONDITION
public static final TextBasedElementBuilder.TypeChoices TIRE_INITIAL_CONDITION
public static final TextBasedElementBuilder.TypeChoices STATIC_VEHICLE_ALIGNMENT
public static final TextBasedElementBuilder.TypeChoices SPRUNG_MASS
public static final TextBasedElementBuilder.TypeChoices USER_DEFINED_FORCE
public static final TextBasedElementBuilder.TypeChoices GLOBAL_DIRECTIONS_LINK_DRIVER
public static final TextBasedElementBuilder.TypeChoices DOT_ONE_LINK_DRIVER
public static final TextBasedElementBuilder.TypeChoices DOT_TWO_LINK_DRIVER
public static final TextBasedElementBuilder.TypeChoices CURVE_ON_CURVE_CONSTRAINT_DRIVER
public static final TextBasedElementBuilder.TypeChoices FIXED_JOINT_DRIVER
public static final TextBasedElementBuilder.TypeChoices LINK_COUPLER_DRIVER
public static final int _THREE_POINT_FORCE
public static final int _THREE_POINT_TORQUE
public static final int _ALL_KINEMATIC_DIRECTION_SENSOR
public static final int _ALL_FORCE_DIRECTION_SENSOR
public static final int _AERO_AERO_FORCE
public static final int _AERO_HYDRO_FORCE
public static final int _AERO_VEHICLE_FORCE
public static final int _CUSTOMIZED_SOLVER
public static final int _STI_TIRE
public static final int _STI_TIRE_PROPERTY
public static final int _BUMP_STOP_CONTACT
public static final int _SPHERE_TO_GROUND_CONTACT
public static final int _GEAR_CONTACT
public static final int _THREE_LINK_SUSPENSION
public static final int _FOUR_LINK_SUSPENSION
public static final int _FIVE_LINK_SUSPENSION
public static final int _ROLL_IAX_SUSPENSION
public static final int _STEER_IAX_SUSPENSION
public static final int _HOTCH_KISS_SUSPENSION
public static final int _MC_PHERSON_SUSPENSION
public static final int _DOUBLE_AARM_SUSPENSION
public static final int _PIVOT_BEAM_SUSPENSION
public static final int _VEHICLE
public static final int _SPEED_SWEEP
public static final int _SYSTEM_PROPERTY
public static final int _DYNAMIC_PROPERTY
public static final int _KINEMATIC_PROPERTY
public static final int _STATIC_PROPERTY
public static final int _PRELOAD_PROPERTY
public static final int _INVERSE_PROPERTY
public static final int _LINEARIZATION_PROPERTY
public static final int _RESTART_PROPERTY
public static final int _ADVANCED_SOLUTION
public static final int _GEAR
public static final int _GENERIC
public static final int _FMI
public static final int _POINT_TO_POINT_CONSTRAINT
public static final int _ORIENTATION_CONSTRAINT
public static final int _FUNCTIONCURVE_CONTROL_INPUT
public static final int _PATH_FOLLOWER_CONTROL_INPUT
public static final int _USER_DEFINED_CONTROL_INPUT
public static final int _SPECIAL_CONTROL_INPUT
public static final int _LINEAR_CONTROL_OUTPUT
public static final int _MASS_PROPERTY_CONTROL_OUTPUT
public static final int _LINK_INITIAL_CONDITION
public static final int _SCREW_JOINT_OR_SPRING_INITIAL_CONDITION
public static final int _FLEXIBLE_LINK_INITIAL_CONDITION
public static final int _TIRE_INITIAL_CONDITION
public static final int _STATIC_VEHICLE_ALIGNMENT
public static final int _SPRUNG_MASS
public static final int _USER_DEFINED_FORCE
public static final int _GLOBAL_DIRECTIONS_LINK_DRIVER
public static final int _DOT_ONE_LINK_DRIVER
public static final int _DOT_TWO_LINK_DRIVER
public static final int _CURVE_ON_CURVE_CONSTRAINT_DRIVER
public static final int _FIXED_JOINT_DRIVER
public static final int _LINK_COUPLER_DRIVER
public static TextBasedElementBuilder.TypeChoices valueOf(int value)
public static TextBasedElementBuilder.TypeChoices valueOf(String name)
public static TextBasedElementBuilder.TypeChoices[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.