public interface MechanismExport extends Remote
MotionSession
Modifier and Type | Interface and Description |
---|---|
static class |
MechanismExport.PositionOrientationFormat
Format to export the position and orientation data.
|
Modifier and Type | Method and Description |
---|---|
void |
exportMdef(String fileName,
MechanismExport.PositionOrientationFormat posOrientFormat,
boolean exportEmptyInputFields,
boolean exportUnusedOptions,
boolean exportSubmechAsMdef,
boolean enablePublish,
String publishedFolder,
NXObject[] objects)
Exports selected objects to .mdef file
License requirements: mechanisms ("MECHANISMS") Created in NX12.0.0 |
void |
exportPlmxml(String fileName,
NXObject[] objects)
Exports Mechanism to .xml file.
|
void exportMdef(String fileName, MechanismExport.PositionOrientationFormat posOrientFormat, boolean exportEmptyInputFields, boolean exportUnusedOptions, boolean exportSubmechAsMdef, boolean enablePublish, String publishedFolder, NXObject[] objects) throws NXException, RemoteException
fileName
- Full path to the .mdef fileposOrientFormat
- Format to export the position and orientation dataexportEmptyInputFields
- When TRUE, exports data that do not have any values definedexportUnusedOptions
- When TRUE, exports data currently unused in the Motion objectsexportSubmechAsMdef
- When TRUE, export the submechanisms as .mdef files. Otherwise references them as .sim files.enablePublish
- When TRUE, the publish option is enabled.publishedFolder
- Full path to the published folderobjects
- Motion objects to exportNXException
RemoteException
void exportPlmxml(String fileName, NXObject[] objects) throws NXException, RemoteException
fileName
- Full path of the .xml fileobjects
- Motion objects or Motion part tagNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.