public static class LinkInitialVelocity.AngularVelocityType extends Enum
MAGNITUDE
is set, LinkInitialVelocity.rotateVector()
and LinkInitialVelocity.rotateExpression()
is valid.If COMPONENT
is selected, LinkInitialVelocity.rotateCsys()
, LinkInitialVelocity.wxExpression()
,
LinkInitialVelocity.wyExpression()
,and LinkInitialVelocity.wzExpression()
is valid.Modifier and Type | Field and Description |
---|---|
static int |
_COMPONENT
Component type define rotate csys
|
static int |
_MAGNITUDE
Magnitude type define rotate vector
|
static LinkInitialVelocity.AngularVelocityType |
COMPONENT
Component type define rotate csys
|
static LinkInitialVelocity.AngularVelocityType |
MAGNITUDE
Magnitude type define rotate vector
|
Modifier and Type | Method and Description |
---|---|
static LinkInitialVelocity.AngularVelocityType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LinkInitialVelocity.AngularVelocityType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LinkInitialVelocity.AngularVelocityType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LinkInitialVelocity.AngularVelocityType MAGNITUDE
public static final LinkInitialVelocity.AngularVelocityType COMPONENT
public static final int _MAGNITUDE
public static final int _COMPONENT
public static LinkInitialVelocity.AngularVelocityType valueOf(int value)
public static LinkInitialVelocity.AngularVelocityType valueOf(String name)
public static LinkInitialVelocity.AngularVelocityType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.