public static class FlexBodyBuilder.Positioning extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ABSOLUTE_ORIGIN
Positioning to absolution place
|
static int |
_COMPONENT_POSITION
Positioning to the place where the component is in assembly
|
static int |
_THREE_POINT_METHOD
Positioning to user defined place using three point method
|
static FlexBodyBuilder.Positioning |
ABSOLUTE_ORIGIN
Positioning to absolution place
|
static FlexBodyBuilder.Positioning |
COMPONENT_POSITION
Positioning to the place where the component is in assembly
|
static FlexBodyBuilder.Positioning |
THREE_POINT_METHOD
Positioning to user defined place using three point method
|
Modifier and Type | Method and Description |
---|---|
static FlexBodyBuilder.Positioning |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlexBodyBuilder.Positioning |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlexBodyBuilder.Positioning[] |
values()
Returns an array that contains the values for this enum.
|
public static final FlexBodyBuilder.Positioning ABSOLUTE_ORIGIN
public static final FlexBodyBuilder.Positioning COMPONENT_POSITION
public static final FlexBodyBuilder.Positioning THREE_POINT_METHOD
public static final int _ABSOLUTE_ORIGIN
public static final int _COMPONENT_POSITION
public static final int _THREE_POINT_METHOD
public static FlexBodyBuilder.Positioning valueOf(int value)
public static FlexBodyBuilder.Positioning valueOf(String name)
public static FlexBodyBuilder.Positioning[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.