public interface WaveLinkRepository extends NXObject
WaveLinkRepository
.
This object performs the task of embedding the link features created by
the command. It also cleans up unused links.
Part.createWavelinkRepository()
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
void |
destroy()
Destroy the link repository
License requirements: None. |
void |
setBuilder(Builder builder)
Set the builder of the active command.If the builder is feat builder,
then the feature from the builder will be queried and used as master feature.
|
void |
setLink(Feature linkFeature)
Set the link created by interpart selection
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
setNonFeatureApplication(boolean flag)
Specify if the client is non-feature based application or not.
|
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getPdmReferenceAttributeValue, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setPdmReferenceAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
void setBuilder(Builder builder) throws NXException, RemoteException
builder
- the builder of the commandNXException
RemoteException
void setLink(Feature linkFeature) throws NXException, RemoteException
linkFeature
- the wavelink featureNXException
RemoteException
void destroy() throws NXException, RemoteException
NXException
RemoteException
void setNonFeatureApplication(boolean flag) throws NXException, RemoteException
flag
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.