public static class ReflectionAnalysisBuilder.ImageMovementTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL
Move image in horizonal direction.
|
static int |
_ROTATE
Rotate image.
|
static int |
_VERTICAL
Move image in vertical direction.
|
static ReflectionAnalysisBuilder.ImageMovementTypes |
HORIZONTAL
Move image in horizonal direction.
|
static ReflectionAnalysisBuilder.ImageMovementTypes |
ROTATE
Rotate image.
|
static ReflectionAnalysisBuilder.ImageMovementTypes |
VERTICAL
Move image in vertical direction.
|
Modifier and Type | Method and Description |
---|---|
static ReflectionAnalysisBuilder.ImageMovementTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReflectionAnalysisBuilder.ImageMovementTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReflectionAnalysisBuilder.ImageMovementTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ReflectionAnalysisBuilder.ImageMovementTypes HORIZONTAL
public static final ReflectionAnalysisBuilder.ImageMovementTypes VERTICAL
public static final ReflectionAnalysisBuilder.ImageMovementTypes ROTATE
public static final int _HORIZONTAL
public static final int _VERTICAL
public static final int _ROTATE
public static ReflectionAnalysisBuilder.ImageMovementTypes valueOf(int value)
public static ReflectionAnalysisBuilder.ImageMovementTypes valueOf(String name)
public static ReflectionAnalysisBuilder.ImageMovementTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.