public static class DisplayPropertiesBuilder.FieldQuantityType extends Enum
Modifier and Type | Method and Description |
---|---|
static DisplayPropertiesBuilder.FieldQuantityType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayPropertiesBuilder.FieldQuantityType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayPropertiesBuilder.FieldQuantityType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE0
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE1
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE2
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE3
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE4
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE5
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE6
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE7
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE8
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE9
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE10
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE11
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE12
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE13
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE14
public static final DisplayPropertiesBuilder.FieldQuantityType TYPE15
public static final int _TYPE0
public static final int _TYPE1
public static final int _TYPE2
public static final int _TYPE3
public static final int _TYPE4
public static final int _TYPE5
public static final int _TYPE6
public static final int _TYPE7
public static final int _TYPE8
public static final int _TYPE9
public static final int _TYPE10
public static final int _TYPE11
public static final int _TYPE12
public static final int _TYPE13
public static final int _TYPE14
public static final int _TYPE15
public static DisplayPropertiesBuilder.FieldQuantityType valueOf(int value)
public static DisplayPropertiesBuilder.FieldQuantityType valueOf(String name)
public static DisplayPropertiesBuilder.FieldQuantityType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.