public static class SeatBeltAnchorageBuilder.LowerLimitType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LENGTH450
lower limit distance of 450
|
static int |
_LENGTH500
lower limit distance of 500
|
static SeatBeltAnchorageBuilder.LowerLimitType |
LENGTH450
lower limit distance of 450
|
static SeatBeltAnchorageBuilder.LowerLimitType |
LENGTH500
lower limit distance of 500
|
Modifier and Type | Method and Description |
---|---|
static SeatBeltAnchorageBuilder.LowerLimitType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeatBeltAnchorageBuilder.LowerLimitType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeatBeltAnchorageBuilder.LowerLimitType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SeatBeltAnchorageBuilder.LowerLimitType LENGTH450
public static final SeatBeltAnchorageBuilder.LowerLimitType LENGTH500
public static final int _LENGTH450
public static final int _LENGTH500
public static SeatBeltAnchorageBuilder.LowerLimitType valueOf(int value)
public static SeatBeltAnchorageBuilder.LowerLimitType valueOf(String name)
public static SeatBeltAnchorageBuilder.LowerLimitType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.