public static class MirrorCertificationBuilder.InstructionFieldPositionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ON_ROAD_SURFACE
Represents that the instrucition field is on road surface
|
static int |
_ON_TARGET_WALL
Represents that the instrucition field is on target wall
|
static MirrorCertificationBuilder.InstructionFieldPositionType |
ON_ROAD_SURFACE
Represents that the instrucition field is on road surface
|
static MirrorCertificationBuilder.InstructionFieldPositionType |
ON_TARGET_WALL
Represents that the instrucition field is on target wall
|
Modifier and Type | Method and Description |
---|---|
static MirrorCertificationBuilder.InstructionFieldPositionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.InstructionFieldPositionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.InstructionFieldPositionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MirrorCertificationBuilder.InstructionFieldPositionType ON_TARGET_WALL
public static final MirrorCertificationBuilder.InstructionFieldPositionType ON_ROAD_SURFACE
public static final int _ON_TARGET_WALL
public static final int _ON_ROAD_SURFACE
public static MirrorCertificationBuilder.InstructionFieldPositionType valueOf(int value)
public static MirrorCertificationBuilder.InstructionFieldPositionType valueOf(String name)
public static MirrorCertificationBuilder.InstructionFieldPositionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.