public static class StiffenerLimitBuilder.LimitType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NEAT_TRIM
It will automatically create an End Cut that trim the stiffener to the selected geometry.
|
static int |
_SQUARE_CUT
Stiffener will extend into limiting geometry.
|
static int |
_VALUE
Trim or extend by a fixed distance value.
|
static StiffenerLimitBuilder.LimitType |
NEAT_TRIM
It will automatically create an End Cut that trim the stiffener to the selected geometry.
|
static StiffenerLimitBuilder.LimitType |
SQUARE_CUT
Stiffener will extend into limiting geometry.
|
static StiffenerLimitBuilder.LimitType |
VALUE
Trim or extend by a fixed distance value.
|
Modifier and Type | Method and Description |
---|---|
static StiffenerLimitBuilder.LimitType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerLimitBuilder.LimitType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerLimitBuilder.LimitType[] |
values()
Returns an array that contains the values for this enum.
|
public static final StiffenerLimitBuilder.LimitType VALUE
public static final StiffenerLimitBuilder.LimitType SQUARE_CUT
public static final StiffenerLimitBuilder.LimitType NEAT_TRIM
public static final int _VALUE
public static final int _SQUARE_CUT
public static final int _NEAT_TRIM
public static StiffenerLimitBuilder.LimitType valueOf(int value)
public static StiffenerLimitBuilder.LimitType valueOf(String name)
public static StiffenerLimitBuilder.LimitType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.