public static class SplitProfilePlateBuilder.SplitDirectionOptionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALONG_PLANE_OR_FACE
Split profile/plate along selected plane or face
|
static int |
_PERPENDICULAR_TO_MOLDING_FACE
create plane/face perpendicular to molding face as the split tool
|
static SplitProfilePlateBuilder.SplitDirectionOptionType |
ALONG_PLANE_OR_FACE
Split profile/plate along selected plane or face
|
static SplitProfilePlateBuilder.SplitDirectionOptionType |
PERPENDICULAR_TO_MOLDING_FACE
create plane/face perpendicular to molding face as the split tool
|
Modifier and Type | Method and Description |
---|---|
static SplitProfilePlateBuilder.SplitDirectionOptionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplitProfilePlateBuilder.SplitDirectionOptionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplitProfilePlateBuilder.SplitDirectionOptionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SplitProfilePlateBuilder.SplitDirectionOptionType PERPENDICULAR_TO_MOLDING_FACE
public static final SplitProfilePlateBuilder.SplitDirectionOptionType ALONG_PLANE_OR_FACE
public static final int _PERPENDICULAR_TO_MOLDING_FACE
public static final int _ALONG_PLANE_OR_FACE
public static SplitProfilePlateBuilder.SplitDirectionOptionType valueOf(int value)
public static SplitProfilePlateBuilder.SplitDirectionOptionType valueOf(String name)
public static SplitProfilePlateBuilder.SplitDirectionOptionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.