public static class SplitProfilePlateBuilder.ProfileType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BUILT_UP
Select built-up as target for split.
|
static int |
_PROFILE_OR_PLATE
Select profile or plate as target for split.
|
static SplitProfilePlateBuilder.ProfileType |
BUILT_UP
Select built-up as target for split.
|
static SplitProfilePlateBuilder.ProfileType |
PROFILE_OR_PLATE
Select profile or plate as target for split.
|
Modifier and Type | Method and Description |
---|---|
static SplitProfilePlateBuilder.ProfileType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplitProfilePlateBuilder.ProfileType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplitProfilePlateBuilder.ProfileType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SplitProfilePlateBuilder.ProfileType PROFILE_OR_PLATE
public static final SplitProfilePlateBuilder.ProfileType BUILT_UP
public static final int _PROFILE_OR_PLATE
public static final int _BUILT_UP
public static SplitProfilePlateBuilder.ProfileType valueOf(int value)
public static SplitProfilePlateBuilder.ProfileType valueOf(String name)
public static SplitProfilePlateBuilder.ProfileType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.