public static class ShipCoordinatesBuilder.Selection extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COMPONENT
Allows routing component selection.
|
static int |
_POINT
Allows point selection.
|
static ShipCoordinatesBuilder.Selection |
COMPONENT
Allows routing component selection.
|
static ShipCoordinatesBuilder.Selection |
POINT
Allows point selection.
|
Modifier and Type | Method and Description |
---|---|
static ShipCoordinatesBuilder.Selection |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipCoordinatesBuilder.Selection |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipCoordinatesBuilder.Selection[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShipCoordinatesBuilder.Selection POINT
public static final ShipCoordinatesBuilder.Selection COMPONENT
public static final int _POINT
public static final int _COMPONENT
public static ShipCoordinatesBuilder.Selection valueOf(int value)
public static ShipCoordinatesBuilder.Selection valueOf(String name)
public static ShipCoordinatesBuilder.Selection[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.