public static class SectionDrawingBuilder.ViewsPerSheetOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FIVE |
static int |
_FOUR |
static int |
_ONE |
static int |
_SIX |
static int |
_THREE |
static int |
_TWO |
static SectionDrawingBuilder.ViewsPerSheetOptions |
FIVE |
static SectionDrawingBuilder.ViewsPerSheetOptions |
FOUR |
static SectionDrawingBuilder.ViewsPerSheetOptions |
ONE |
static SectionDrawingBuilder.ViewsPerSheetOptions |
SIX |
static SectionDrawingBuilder.ViewsPerSheetOptions |
THREE |
static SectionDrawingBuilder.ViewsPerSheetOptions |
TWO |
Modifier and Type | Method and Description |
---|---|
static SectionDrawingBuilder.ViewsPerSheetOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionDrawingBuilder.ViewsPerSheetOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionDrawingBuilder.ViewsPerSheetOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final SectionDrawingBuilder.ViewsPerSheetOptions ONE
public static final SectionDrawingBuilder.ViewsPerSheetOptions TWO
public static final SectionDrawingBuilder.ViewsPerSheetOptions THREE
public static final SectionDrawingBuilder.ViewsPerSheetOptions FOUR
public static final SectionDrawingBuilder.ViewsPerSheetOptions FIVE
public static final SectionDrawingBuilder.ViewsPerSheetOptions SIX
public static final int _ONE
public static final int _TWO
public static final int _THREE
public static final int _FOUR
public static final int _FIVE
public static final int _SIX
public static SectionDrawingBuilder.ViewsPerSheetOptions valueOf(int value)
public static SectionDrawingBuilder.ViewsPerSheetOptions valueOf(String name)
public static SectionDrawingBuilder.ViewsPerSheetOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.