public static class PlateChamferBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ON_EDGE
Create a chamfer on the edge
|
static int |
_TO_PLATE
Create a chamfer on the common edges between plates
|
static PlateChamferBuilder.Types |
ON_EDGE
Create a chamfer on the edge
|
static PlateChamferBuilder.Types |
TO_PLATE
Create a chamfer on the common edges between plates
|
Modifier and Type | Method and Description |
---|---|
static PlateChamferBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateChamferBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateChamferBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final PlateChamferBuilder.Types ON_EDGE
public static final PlateChamferBuilder.Types TO_PLATE
public static final int _ON_EDGE
public static final int _TO_PLATE
public static PlateChamferBuilder.Types valueOf(int value)
public static PlateChamferBuilder.Types valueOf(String name)
public static PlateChamferBuilder.Types[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.