public static class EdgeCutBuilder.VersionID extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NX85
This feature builder is used to edit an existing NX85 - NX9 edge cut feature.
|
static int |
_NX901
This feature builder is used to create or edit an NX901 or beyond feature.
|
static EdgeCutBuilder.VersionID |
NX85
This feature builder is used to edit an existing NX85 - NX9 edge cut feature.
|
static EdgeCutBuilder.VersionID |
NX901
This feature builder is used to create or edit an NX901 or beyond feature.
|
Modifier and Type | Method and Description |
---|---|
static EdgeCutBuilder.VersionID |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeCutBuilder.VersionID |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeCutBuilder.VersionID[] |
values()
Returns an array that contains the values for this enum.
|
public static final EdgeCutBuilder.VersionID NX85
public static final EdgeCutBuilder.VersionID NX901
public static final int _NX85
public static final int _NX901
public static EdgeCutBuilder.VersionID valueOf(int value)
public static EdgeCutBuilder.VersionID valueOf(String name)
public static EdgeCutBuilder.VersionID[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.