public static class JogBuilder.BendLocationOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BEND_OUTSIDE |
static int |
_MATERIAL_INSIDE |
static int |
_MATERIAL_OUTSIDE |
static JogBuilder.BendLocationOptions |
BEND_OUTSIDE |
static JogBuilder.BendLocationOptions |
MATERIAL_INSIDE |
static JogBuilder.BendLocationOptions |
MATERIAL_OUTSIDE |
Modifier and Type | Method and Description |
---|---|
static JogBuilder.BendLocationOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JogBuilder.BendLocationOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JogBuilder.BendLocationOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final JogBuilder.BendLocationOptions MATERIAL_INSIDE
public static final JogBuilder.BendLocationOptions MATERIAL_OUTSIDE
public static final JogBuilder.BendLocationOptions BEND_OUTSIDE
public static final int _MATERIAL_INSIDE
public static final int _MATERIAL_OUTSIDE
public static final int _BEND_OUTSIDE
public static JogBuilder.BendLocationOptions valueOf(int value)
public static JogBuilder.BendLocationOptions valueOf(String name)
public static JogBuilder.BendLocationOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.